MITSUBISHI ELECTRIC Changes for the Better
Africa
MELSOFT VIXIO is a software that performs visual inspection in coordination with external devices such as cameras. All necessary functions for a visual inspection system can be set up easily without programming.

What is MELSOFT VIXIO?

Youtube

Please accept functional cookies to watch our YouTube videos.

Concerns in the inspection process:

  • Labor shortages increase the burden on inspectors
  • Generational changes in inspectors make consistent visual inspection difficult
  • Even though inspection is rule-based, overdetection is increasing

MELSOFT VIXIO application examples

Combination of rule-based and AI-based inspections

Introducing MELSOFT VIXIO AI inspection and using it together with existing rule-based inspection improves inspection accuracy.

Perform primary screening with AI

Checking products identified in primary screening based on AI judgment results (heat map) reduces task labor.

Double check by AI and human eyes

The introduction of doublechecking reduces the risk of overlooking defective products and ensures consistency of quality between operators.

Featuring a high-speed, high-precision AI algorithm ideal for factory automation

Even unexpected defects can be detected.

  • AI introduction challenge

The limited number of defective product images complicates accuracy improvement. Generating AI models requires extensive image learning, making the process time consuming and inefficient.

  • With MELSOFT VIXIO

Easily generate AI models with high-speed, high-accuracy AI.

Detection of similar defects even in different locations or with different sizes is possible.

  • Defective point detection

AI that detects defects! Detect specific abnormality patterns. Model generation from even a single defective product image. 

Operation processes

Learning phase

Step 1: Organize & Categorize 

Gather images of both good and bad quality products and categorize them accordingly. This can involve using existing archived images or installing a camera on the production line to capture real-time images during production.

Step 2: Preprocess Images

Adjust the images through preprocessing techniques to optimize them for analysis by the AI. This may include tasks such as cropping out irrelevant areas to focus only on the pertinent parts needed for analysis.

Step 3: AI Model Creation With just a click of a button

Initiate the creation of the AI model. The AI utilizes a subset of the provided images for training the model and another subset for validating its performance. This streamlined process ensures the swift development and deployment of the AI for product quality analysis, allowing for transparent evaluation of its effectiveness and performance.

Inspection phase

Step 4: Configure the Task

Leverage pre-designed templates in low-code platforms to effortlessly configure the hardware and software setup. Define the interactions between the Programmable Logic Controller (PLC), MELSOFT VIXIO, and camera with ease. Direct integration of GigE Vision® cameras allows easy configuration and fine-tuning.

Step 5
: Real-time Operation on the Production Line

Initiate the task on the production machine to commence real-time quality analysis. Gain immediate access to a live heatmap visualization of product quality, providing instant insights into production performance. Seamlessly track inspection history for comprehensive traceability functions, ensuring continuous improvement and quality control.

System Requirements

Check the required operating environment for the visual inspection software MELSOFT VIXIO.

License system

Development license*

Period of useRemarks
1 yearAll functions can be used
ItemRecommendedMinimum
CPUIntel® Core-i7™ 9th generation (October 2018) or higherIntel® Core-i5™ 9th generation (October 2018) or higher
GPUNVIDIA GPU Ampere Architecture or higherMemory: 8 GB or moreNVIDIA GPU Pascal™ Architecture or higherMemory: 6 GB or more
Memory32 GB or more16 GB or more
OS (64-bit version)Microsoft® Windows® 10 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 11 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 10 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 11 Version 21H2 or later (Pro, Enterprise)
Free storage space512 GB or more256 GB or more

Run-time license*

Period of useRemarks
Perpetual (one-time purchase)Functions other than AI modelgeneration can be used
ItemRecommendedMinimum
CPUIntel® Core-i7™ 9th generation (October 2018) or higheIntel® Core-i5™ 9th generation (October 2018) or higher
GPUNVIDIA GPU Pascal™ Architecture or higherMemory: 6 GB or moreNVIDIA GPU Pascal™ Architecture or higherMemory: 4 GB or more
Memory16 GB or more8 GB or more
OS (64-bit version)Microsoft® Windows® 10 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 11 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 10 Version 21H2 or later (Pro, Enterprise)Microsoft® Windows® 11 Version 21H2 or later (Pro, Enterprise)
Free storage space256 GB or more128 GB or more

*:Node-locked license for one computer

Connectable industrial camera specifications

Hardware standardsSoftware standards
Conforms to GigE Vision® (Ver. 2.0)Conforms to GenICam™ (Ver. 3.2.0)

Note 1: For information on usable industrial cameras, please refer to Technical Bulletin FA-A-0419.

Note 2: “Connectable” means the following:

· Camera-side parameters (exposure time or white balance) can be adjusted in this product.
· Image capture command can be issued directly by this product. 

Since it is possible to browse to a folder on the computer and perform AI inspection on stored images, cameras which do not meet the above specifications can also be used.

How to install

Partner

MELSOFT VIXIO sales partners are companies equipped with comprehensive product knowledge and support capabilities for MELSOFT VIXIO. You can rely on them for assistance ranging from optical evaluation to system upgrades. For inquiries concerning MELSOFT VIXIO, please reach out to the partner companies listed below.

Area

Comming Soon

30-day trial of MELSOFT Vixio

Select...
The fields marked by a * are mandatory.